Everything

R_FMC_Set_PowerOff

Halts the clock supplied to the subsystem clock frequency measurement circuit.

Remark         Calling this API function changes the subsystem clock frequency measurement circuit to reset status.
For this reason, writes to the control registers after this API function is called are ignored.

 

[Syntax]

void    R_FMC_Set_PowerOff ( void );

 

[Argument(s)]

None.

 

[Return value]

None.