Everything

r_lvd_exlvdinterrupt

Performs processing in response to the voltage detection of EXLVD pin interrupt INTLVDEXLVD.

Remark         This API function is called as the interrupt process corresponding to the voltage detection of EXLVD pin interrupt INTLVDEXLVD.

 

[Syntax]

CA78K0R Compiler

__interrupt static void   r_lvd_exlvdinterrupt ( void );

 

CC-RL Compiler

static void   __near r_lvd_exlvdinterrupt ( void );

 

[Argument(s)]

None.

 

[Return value]

None.