Performs processing in response to the voltage detection of VBAT pin interrupt INTLVDVBAT.
Remark This API function is called as the interrupt process corresponding to the voltage detection of VBAT pin interrupt INTLVDVBAT.
[Syntax]
CA78K0R Compiler
__interrupt static void r_lvd_vbatinterrupt ( void );
CC-RL Compiler
static void __near r_lvd_vbatinterrupt ( void );
[Argument(s)]
None.
[Return value]
None.