Performs processing in response to the voltage detection of VDD pin interrupt INTLVDVDD.
Remark This API function is called as the interrupt process corresponding to the voltage detection of VDD pin interrupt INTLVDVDD.
[Syntax]
CA78K0R Compiler
__interrupt static void r_lvd_vddinterrupt ( void );
CC-RL Compiler
static void __near r_lvd_vddinterrupt ( void );
[Argument(s)]
None.
[Return value]
None.