Performs processing in response to the 32-bit Multiply-accumulator interrupt INTMACLOF.
Remark This API function is called as the interrupt process corresponding to the 32-bit Multiply-accumulator interrupt INTMACLOF.
[Syntax]
CA78K0R Compiler
__interrupt static void r_mac32bit_interrupt_flow ( void );
CC-RL Compiler
static void __near r_mac32bit_interrupt_flow ( void );
[Argument(s)]
None.
[Return value]
None.