Operates the unsigned multiply-accumulate.
[Syntax]
#include “r_cg_macrodriver.h”
#include “r_cg_mac32bit.h”
void R_MAC32Bit_MACUnsigned ( uint32_t data_a, uint32_t data_b, mac32bit_uint64_t
* buffer_64bit );
[Argument(s)]
I/O |
Argument |
Description |
I |
uint32_t data_a; |
Multiplicand |
I |
uint32_t data_b; |
Multiplier |
O |
mac32bit_uint64_t * buffer_64bit; |
Accumulation initial value / Multiplier result |
Remark See R_MAC32Bit_MULUnsigned for details about the mac32bit_uint64_t.
None.