32-bit Multiply-accumulator
Below is a list of API functions output by the Code Generator for 32-bit Multiply-accumulator use.
Table 3.48 API Functions: [32-bit Multiply-accumulator]
API Function Name |
Function |
Performs initialization necessary to control the 32-bit Multiply-accumulator. | |
Performs user-defined initialization relating to the 32-bit Multiply-accumulator. | |
Performs processing in response to the 32-bit Multiply-accumulator interrupt INTMACLOF. | |
Resets the 32-bit Multiply-accumulator. | |
Stops the cock supplied for the 32-bit Multiply-accumulator. | |
Operates the unsigned multiply. | |
Operates the signed multiply. | |
Operates the unsigned multiply-accumulate. | |
Operates the signed multiply-accumulate. |