Everything

r_smotd_counterA_interrupt

Performs processing in response to the Sampling output timer interval interrupt INTSMOTA.

Remark         This API function is called as the interrupt process corresponding to the Sampling output timer interval interrupt INTSMOTA.

 

[Syntax]

CA78K0R Compiler

__interrupt static void    r_smotd_interrupt ( void );

 

CC-RL Compiler

static void    __near r_smotd_interrupt ( void );

 

[Argument(s)]

None.

 

[Return value]

None.