Everything

Sampling output timer detector

Below is a list of API functions output by the Code Generator for Sampling output timer detector use.

 

Table 3.53      API Functions: [Sampling output timer detector]

API Function Name

Funciton

R_SMOTD_Create

Performinitialization necessary to control the Sampling output timer detector.

R_SMOTD_Create_UserInit

Performs user-defined initialization relating to the Sampling output timer detector.

r_smotd_counterA_interrupt

Performs processing in response to the Sampling output timer interval interrupt INTSMOTA.

r_smotd_counterB_interrupt

performs processing in response to the Sampling output timer compare match interrupt INTSMOTB.

r_smotd_smpn_interrupt

Performs processing int response to the Sampling detector detection interrupt INTSMPn.

R_SMOTD_Start

Start Starts Sampling output timer detector.

R_SMOTD_Stop

Ends Sampling output timer detector.

R_SMOTD_Set_PowerOff

Halts the clock supplied to the Sampling output timer detector.