Everything

r_smotd_smpn_interrupt

Performs processing in response to the Sampling detector detection interrupt INTSMPn.

Remark         This API function is called as the interrupt process corresponding to the Sampling detector detection interrupt INTSMPn.

 

[Syntax]

CA78K0R Compiler

__interrupt static void    r_smotd_smpn_interrupt ( void );

 

CC-RL Compiler

static void    __near r_smotd_smpn_interrupt ( void );

Remark         n is the sampling input number.

 

[Argument(s)]

None.

 

[Return value]

None.