Everything

R_TAUm_Channeln_Higher8bits_Stop

Ends the count (higher 8-bit) for channel n.

Remark         This API function can only be called when the timer array unit is used as a 8-bit timer.

 

[Syntax]

void       R_TAUm_Channeln_Higher8bits_Stop ( void );

Remark         m is the unit number, and n is the channel number.

 

[Argument(s)]

None.

 

[Return value]

None.