Everything

R_TAUm_Channeln_Start

Starts the count for channel n.

Remark         The time from the call to this API function to the start of counting depends on the type of the function in question (e.g. interval timer, square-wave output, or external event counter).

 

[Syntax]

void       R_TAUm_Channeln_Start ( void );

Remark         m is the unit number, and n is the channel number.

 

[Argument(s)]

None.

 

[Return value]

None.