Everything

r_taum_channeln_interrupt

Performs processing in response to the timer interrupt INTTMmn.

Remark         This API function is called as the interrupt process corresponding to the timer interrupt INTTMmn.

 

[Syntax]

CA78K0R Compiler

__interrupt static void   r_taum_channeln_interrupt ( void );

 

CC-RL Compiler

static void   _near r_taum_channeln_interrupt ( void );

Remark         m is the unit number, and n is the channel number.

 

[Argument(s)]

None.

 

[Return value]

None.