Everything

r_elc_elsrni_interrupt

Performs processing in response to the event link interrupt.

Remark         This API function is called to run interrupt processing for the event signal defined in event link setting register.
n is the source number.

 

[Syntax]

static void    r_elc_elsrni_interrupt ( void );

Remark         n is the source number.

 

[Argument(s)]

None.

 

[Return value]

None.