Gets the value of a port
buffer.
[Syntax]
void
R_ELC_Get_PortBuffern ( uint8_t * const value );
Remark
n is the source number.
[Argument(s)]
I/O |
Argument |
Description |
O |
uint8_t * const
value; |
Pointer to the
location where the obtained value is to be
stored. |
[Return
value]
None.