Everything

Event link controller (ELC)

Below is a list of API functions output by the Code Generator for event link controller use.

 

Table 3.10 API Functions: [Event Link Controller]

API Function Name

Function

R_ELC_Create

Performs initialization necessary to control the event link controller.

R_ELC_Create_UserInit

Performs user-defined initialization relating to the event link controller.

r_elc_elsrni_interrupt

Performs processing in response to the event link interrupt.

R_ELC_Start

Starts interlinked operation of peripheral functions.

R_ELC_Stop

Ends interlinked operation of peripheral functions.

R_ELC_GenerateSoftwareEvent

Generates the software event.

R_ELC_Set_PortBuffern

Sets the value of a port buffer.

R_ELC_Get_PortBuffern

Gets the value of a port buffer.