Everything

[RI850V4] tab

Outline
This tab shows the detailed information on RI850V4 to be used categorized by the following.
- Version Information
This tab can be opened as follows:
- On the Project Tree panel, select a component such as the Realtime OS node or the system configuration file, and then select the [View] menu -> Property] or select [Property] from the context menu.
Note When the Property panel is already open, selecting a component such as the Realtime OS node or the system configuration file on the Project Tree panel displays the detailed information regarding the selected component.
Display image
Explanation of each area
1 ) [Version Information]
The detailed information on the version of the RI850V4 are displayed.
Kernel version
Display the version of RI850V4 to be used.
Default
The latest version of the installed RI850V4 package
How to change
Changes not allowed
Install folder
Display the folder in which RI850V4 to be used is installed with the absolute path.
Default
The folder in which RI850V4 to be used is installed
How to change
Changes not allowed
Register mode
Display the register mode set in the project.
Display the same value as the value of the [Select register mode] property of the build tool.
Default
The register mode selected in the property of the build tool
How to change
Changes not allowed