Everything

APPENDIX A WINDOW REFERENCE


This appendix explains the window/panels that are used when the activation option for the CF850V4 is specified from the integrated development environment platform CS+.
A.1 Description
The following shows the list of window/panels.
Table A-1 List of Window/Panels
Window/Panel Name
Function Description
This is the first window to be opened when CS+ is launched.
This window is used to manipulate the CS+ components (such as the build tool and resource information tool).
This panel is used to display the project components (such as the microcontroller and build tool) in tree view.
This panel is used to display information regarding the node selected on the Project Tree panel and change the settings of the information.