Everything

Main window

Outline
This is the first window to be opened when CS+ is launched. This window is used to manipulate the CS+ components (such as the build tool and resource information tool).
This window can be opened as follows:
- Select Windows [start] -> [All programs] -> [Renesas Electronics CS+] -> [CS+ for CC (RL78, RX, RH850)]
Display image
Explanation of each area
1 ) Menu bar
This area contains the following group of menus.
- [View] menu
Realtime OS
The [View] menu shows the cascading menu to start the tools of Real-Time OS.
Resource Information
Opens the Realtime OS Resource Information panel.
Note that this menu is disabled when the debug tool is not connected.
Performance Analyzer
This menu is always disabled.
Task Analyzer 1
Opens the Realtime OS Task Analyzer 1 panel.
Note that this menu is disabled when the debug tool is not connected.
Task Analyzer 2
Opens the Realtime OS Task Analyzer 2 panel.
Note that this menu is disabled when the debug tool is not connected.

2 ) Toolbar
Displays the buttons relate to Realtime OS.
Buttons on the toolbar can be customized in the User Setting dialog box. You can also create a new toolbar in the same dialog box.
- Realtime OS toolbar
Opens the Realtime OS Resource Information panel.
Note that this button is disabled when the debug tool is not connected.
Opens the Realtime OS Task Analyzer 1 panel.
Note that this menu is disabled when the debug tool is not connected.
Opens the Realtime OS Task Analyzer 2 panel.
Note that this menu is disabled when the debug tool is not connected.

3 ) Panel display area
The following panels are displayed in this area.
- Output panel
See the each panel section for details of the contents of the display.
Note See CS+ Integrated Development Environment User's Manual: Build for details about the Output panel.