Everything

 

-Xintermodule


This option performs inter-module optimization.

[Specification format]

-Xintermodule

 

-

Interpretation when omitted

Inter-module optimization is not performed.

[Detailed description]

-

This option performs inter-module optimization.

-

The main optimization contents are shown below.

-

Optimization using inter-procedural alias analysis

The example of the output code is shown below.

[C source]
extern int x[2];
static int func1(int *a, int *b) {
    *a=0;
    *b=1;
    return *a;
}
int func2() {
    return func1(&x[0], &x[1]);
}
 
[Output assembler source]
_func1.1:
    .stack  _func1.1 = 0
    mov     #_x, r2
    st.w    r0, 0x00000000[r2]
    mov     0x00000001, r5
    st.w    r5, 0x00000004[r2]
    mov     0x00000000, r10     ; 0 is directly assigned because a and b point to different addresses.
    jmp     [r31]
_func2:
    .stack  _func2 = 0
    mov     #_x, r6
    addi    0x00000004, r6, r7
    br9     _func1.1

 

-

Constant propagation of parameters and return values

The example of the output code is shown below.

[C source]
static int func(int x, int y, int z) {
    return x-y+z;
}
int func2() {
    return func(3,4,5);
}
 
[Output assembler source]
_func.1:
    .stack  _func.1 = 0
    mov     0x00000000, r10     ; "4(=3-4+5)" is assigned directly.
    jmp     [r31]
_func2:
    .stack  _func2 = 0
    mov     0x00000005, r8
    mov     0x00000004, r7
    mov     0x00000003, r6
    br9     _func.1

[Example of use]

-

To perform inter-module optimization on source files "main.c" and "sub.c", describe as:

>ccrh -Xintermodule -Osize -Xcommon=rh850 main.c sub.c