This option performs optimization with consideration for the type of the data indicated by the pointer.
Optimization with consideration for the type of the data indicated by the pointer, based on the ANSI standard is not performed.
This option specifies whether to perform optimization with consideration for the type of the data indicated by the pointer, based on the ANSI standard. |
The items that can be specified as value are shown below. |
To perform optimization with consideration for the type of the data indicated by the pointer, based on the ANSI standard, describe as: |