This option performs inline expansion of standard library functions "strcpy", "strcmp", "memcpy", and "memset" calls.
Inline expansion of standard library functions "strcpy", "strcmp", "memcpy", and "memset" calls is not performed.
This option performs inline expansion of standard library functions "strcpy", "strcmp", "memcpy", and "memset" calls. |
If this option is specified, arrays and character strings are allocated automatically to 4-byte boundary area. |
To perform inline expansion of standard library functions "strcpy", "strcmp", "memcpy", and "memset" calls, describe as: |