This option specifies the data size of double and long double type.
[Specification format]
- | Interpretation when omitted |
double and long double type are 8 bytes (this is the same result as when -Xdbl_size=8 is specified).
[Detailed description]
- | This option specifies the data size of double and long double type. |
- | One of the following can be specified as num. An error will occur if any other item is specified. |
- | 4
double and long double type are 4 bytes. |
- | 8
double and long double type are 8 bytes. |