Everything

 

-Xcheck_exclusion_control [V1.04.00 or later]


This option is used to select checking of exclusive control.

[Specification format]

-Xcheck_exclusion_control=<filename>

 

-

Interpretation when omitted

Checking of exclusive control is disabled.

[Detailed description]

-

This option loads the setting file and inserts the dbtag instruction at the specified location.

-

This function assumes usage via CS+ and it should not be used directly by the user.