Everything

 

-LIB_REName [V2.01.00 or later]


This option changes a symbol name or section name that was input from a library.

[Specification format]

-lib_rename = name1=name2[, ...]
-lib_rename = file(name1=name2[, ...])
-lib_rename = "file|module[|module ...](name1=name2[, ...])"

 

-

Interpretation when omitted

None

[Detailed description]

-

This option changes the name of an external symbol or section included in a module within the library that was specified by the -library option.

-

Specify the symbol name or section name to be changed as name1. Specify the symbol name or section name after the change as name2.

-

When you specify a C variable name, add prefix "_" to the definition name in the program.

-

If the specified name matches both section and symbol names, the symbol name is changed.

-

If there are two or more files or modules with the same name, the priority depends on the input order.

-

If this option is specified more than once, all specifications will be valid.

-

An error will occur in any of the following cases.

-

When the specified name, file, or module cannot be found

-

When the parameter is omitted

-

When this option is specified together with the -form={object,library}, -extract, or -strip option

[Remark]

-

When the -form={absolute|hexadecimal|stype|binary} option is specified, the -show=struct option cannot be specified together.

-

The section name of the input library cannot be changed.

-

Correct operation is not guaranteed if this option is used in combination with the compiler option -Xmerge_files.

[Example of use]

-

To change "_sym1" in b.lib and c.lib to "_data", describe as:

>rlink a.obj -lib=b.lib,c.lib  -lib_rename=(_sym1=_data)

-

To change "_sym1" in all modules in b.lib to "_data", describe as:

>rlink a.obj -lib=b.lib,c.lib  -lib_rename=b.lib(_sym1=_data)

-

To change "_sym1" in modules m1 and m2 in b.lib to "_data", describe as:

>rlink a.obj -lib=b.lib,c.lib  -lib_rename="b.lib|m1|m2(_sym1=_data)"