Everything

 

-CHange_message


This option changes the type of information, warning, and error messages.

[Specification format]

-CHange_message=suboption [ , ...]
  suboption := level
            |  level=range[, ...]
  range := num
        |  num-num

 

-

Interpretation when omitted

None

[Detailed description]

-

This option changes type level of information, warning, and error messages.

-

The execution continuation or abort at the message output.

-

The items that can be specified as level are shown below.

Information

Information

Warning

Warning

Error

Error

 

-

If message number num is specified, the type of the message with the specified number is changed.
Also, a range of message numbers can be specified using a hyphen (-).

-

Specify the 4-digit number that is output after the component number (05) and the phase of occurrence (6) as num (for example, specify 2310 for message number E0562310).

-

If the specification of a message number is omitted, the types of all messages are changed to the specified one.

[Example of use]

-

To change "E0561310" to a warning and continue the execution at the "E0561310" output, describe as:

>rlink a.obj b.obj -change_message=warning=1310

 

-

To change all information and warning messages to error messages, describe as:
If a message is output, the execution will abort.

>rlink a.obj b.obj -change_message=error