Everything

 

-STRip


This option deletes debug information in the load module file or library file.

[Specification format]

-STRip

 

-

Interpretation when omitted

None

[Detailed description]

-

This option deletes debug information in the load module file or library file.

-

The files before debug information is deleted are backed up in file "file-name.abk".

-

If this option is specified, one input file should correspond to one output file.

[Example of use]

-

To delete debug information of file1.abs, file2.abs, and file3.abs, and output these to file1.abs, file2.abs, and file3.abs, respectively, describe as:

The files before debug information is deleted are backed up in file1.abk, file2.abk, and file3.abk.

<Command line>

>rlink -subcommand=sub.txt

 

<Subcommand file "sub.txt">

-input=file1.abs file2.abs file3.abs
-strip

[Remark]

-

If the -form={object|relocate|hexadecimal|stype|binary} option is specified, this option will be invalid.