Everything
5.3.1 Outline

Control instructions provide detailed instructions for assembler operation and so are written in the source.

Control instructions do not become the target of object code generation.

Control instruction categories are displayed below.

Table 5.15

Control Instruction List

 

As with directives, control instructions are specified in the source.