Everything
5.3.2 Assembler control instructions

The assembler control instruction can be used to control the processing performed by the assembler.

The following assembler control instructions are available.

Table 5.16

Assembler Control Instructions

Control Instruction

Overview

REG_MODE

Outputs a register mode information

NOMACRO

Does not expand the subsequent instructions

MACRO

Cancels the specification made with the NOMACRO directive

DATA

Assumes that external data having symbol name extern_symbol has been allocated neither sdata nor sbss attribute section, and expands the instructions which reference that data

SDATA

Assumes that external data having symbol name extern_symbol has been allocated to the sdata or sbss attribute section, and dose not expand the instructions which reference that data

NOWARNING

Does not output warning messages

WARNING

Output warning messages