5.3.3
File input control instructions
Using the file input control instruction, the assembler can input an assembler source file or binary file to a specified position.
The following file input control instructions are available.
Table 5.17 | File Input Control Instructions |
|
|
INCLUDE
|
Quotes a series of statements from another source module file
|
BINCLUDE
|
Inputs a binary file
|