Output character string to stream
Remark | These functions are not supported by the debugging functions which CS+ provides. |
[Classification]
Standard library
[Syntax]
#include <stdio.h>
int fputs(const char *s, FILE *stream);
[Return value]
0 is returned.
Error return does not occur.
[Description]
This function outputs the string s to the output stream pointed to by stream. The end-of-string null character is not output. Only the standard input/output stdout or stderr can be specified for stream.