Read one character from standard input
Remark | These functions are not supported by the debugging functions which CS+ provides. |
[Classification]
Standard library
[Syntax]
#include <stdio.h>
int getchar(void);
[Return value]
The input character is returned.
Error return does not occur.
[Description]
This function inputs one character from the standard input/output stdin.