Everything

puts


Output character string to standard output stream

Remark

These functions are not supported by the debugging functions which CS+ provides.

[Classification]

Standard library

[Syntax]

#include <stdio.h>

int puts(const char *s);

[Return value]

0 is returned.

Error return does not occur.

[Description]

This function outputs the string s to the standard input/output stdout. The end-of-string null character is not output, but a new-line character is output in its place.