Clock generation circuit
Below is a list of API functions output by the Code Generator for clock generation circuit use.
Table 3.2 API Functions: [Clock Generation Circuit]
|
API Function Name |
Function |
|
Performs initialization required to control the clock generation circuit. | |
|
Performs user-defined initialization relating to the clock generation circuit. | |
|
Performs processing in response to the osillation stop detection interrupt. | |
|
Performs processing in response to the oscillation stop detection NMI. | |
|
Sets the clock source. |