Data operation circuit (DOC)
Below is a list of API functions output by the Code Generator for data operation circuit.
Table 3.34 API Functions: [Data Operation Circuit]
| 
       API Function Name  | 
    
       Function  | 
| 
       Performs initialization necessary to control the data operation circuit.  | |
| 
       Performs user-defined initialization relating to the data operation circuit.  | |
| 
       Performs processing in response to the data operation circuit interrupt.  | |
| 
       Sets the operating mode and the initial value of the reference value for use by the data operation circuit.  | |
| 
       Sets the input value (value for comparison with, addition to, or subtraction from the reference value) for use by the data operation circuit.  | |
| 
       Gets the result of operation.  | |
| 
       Clears the data operation circuit flag.  |