Common
Below is a list of API functions output by the Code Generator for common use.
Performs processing in response to the exception (other than undefined instruction exception, reset, non-maskable
interrupt and unconditional trap).
Table 3.1 API Functions: [Common]
| 
       API Function Name  | 
    
       Function  | 
| 
       Performs processing in response to the undefined instruction exception.  | |
| 
       Performs processing in response to the reset.  | |
| 
       Performs processing in response to the reset.  | |
| 
       Performs processing in response to the privileged instruction exception.  | |
| 
       Performs processing in response to the floating-point exception.  | |
| 
       Performs processing in response to the access exception.  | |
| 
       Performs processing in response to the non-maskable interrupt.  | |
| 
       Performs processing in response to the unconditional trap.  | |
| 
       Performs processing in response to the exception (other than undefined instruction exception, reset, non-maskable interrupt and unconditional trap).  | |
| 
       Performs initialization necessary to control the various hardwares.  | |
| 
       Performs initialization necessary to control the various peripheral functions.  | |
| 
       This is a main function.  | |
| 
       Performs user-defined initialization.  | |
| 
       Performs processing in response to the group interrupt.  | |
| 
       Performs processing in response to the non-maskable interrupt.  | |
| 
       Performs initialization necessary to control the various hardwares.  |