Everything
2.12.1.2 [Simulator]

This timer operation can be configured in the [Trace] category on the [Debug Tool Settings] tab in the Property panel.

Figure 2.86

[Timer] Category [Simulator]

(1)

[Use timer function]

Select whether to use the timer function.

Select [Yes] to use the timer function (default: [No]).