Everything
2.12.1 Configure the timer operation

Before the timer function can be used, it is necessary to make settings relating to the operation of a timer.

Note that the method on how to set differs depending on the debug tool used.

 

2.12.1.1 [IECUBE]

2.12.1.2 [Simulator]