In the program execution process, the execution time in a section can be measured by setting Timer Result event. This Timer Result event consists of a timer start event and a timer end event.
To use this function, follow the procedure described below.
2.12.3.1 Set a Timer Result event
2.12.3.3 Edit a Timer Result event
2.12.3.4 Delete a Timer Result event
Also see "2.15.7 Notes for setting events" for details on Timer Result events (e.g. limits on the number of enabled events). |