Everything
2.12.4 Measurable time ranges

The scope of time that can be measured via timers using Run-Break Timer events (see "2.12.2 Measure execution time until stop of the execution" for details) or Timer Result events (see "2.12.3 Measure execution time in a section [IECUBE][Simulator]" for details) is shown below.

If the maximum measurable length of time is exceeded, a timer-over break is generated, and program execution stops.

Table 2.15

Measurable Time Ranges

Debug Tool

Run-Break Timer Event

Timer Result Event

IECUBE

Min.

8 ns

Min.

8 ns

Max.

Approx. 40 hours 43 min

Overflow detection included

Max.

Approx. 40 hours 43 min (time for 4K cycles)

Maximum pass count: 4294967295 times

Overflow detection included

E1/E20
EZ Emulator

Min.

100 μs

-

Max.

Approx. 119 hours 18 min

Simulator

Depends on the clock frequency for timer/trace

Depends on the clock frequency for timer/trace