|
build.Compile.OutputAssemblySourceFile
|
This property is for setting or referring to whether to output assembly source files. It is a compile option for the active project.
[Specification format]
build.Compile.OutputAssemblySourceFile = bool
|
[Setting(s)]
|
|
|
|
bool
|
Set whether to output assembly source files.
True: Output assembly source files.
False: Do not output assembly source files.
|
[Reference]
If assembly source files are to be output: True
If assembly source files are not to be output: False
[Detailed description]
- | This property is for setting or referring to whether to output assembly source files. It is a compile option for the active project. |
[Example of use]
>>>build.Compile.OutputAssemblySourceFile = True
>>>print build.Compile.OutputAssemblySourceFile
True
>>>
|