|
build.Link.SectionROMtoRAM
|
This property sets or refers to the link options for the active project regarding sections where symbols are mapped from ROM to RAM. [CC-RH][CC-RX][CC-RL]
[Specification format]
build.Link.SectionROMtoRAM = sectionlist
|
[Setting(s)]
|
|
|
|
sectionlist
|
Set the section that maps symbols from ROM to RAM as a list of strings.
|
[Reference]
List of the section that maps symbols from ROM to RAM
[Detailed description]
- | This property sets or refers to the link options for the active project regarding sections where symbols are mapped from ROM to RAM. |
- | Add or change for the referred list to change the setting. |
[Example of use]
>>>sec = build.Link.SectionROMtoRAM ... Refer the current setting and add the section that maps symbols from ROM to RAM
>>>print sec
['D=R', 'D_1=R_1', 'D_2=R_2']
>>>sec.append('D_3=R_3')
>>>build.Link.SectionROMtoRAM = sec
>>>print build.Link.SectionROMtoRAM
['D=R', 'D_1=R_1', 'D_2=R_2', 'D_3=R_3']
|