|
build.ROMization.OutputObjectFile
|
This property sets or refers to the setting for output of a ROMized object file, that is, the value of the ROMization process option for the active project. [CA850][CX][CA78K0R]
[Specification format]
build.ROMization.OutputObjectFile = bool
|
[Setting(s)]
|
|
|
|
bool
|
Set whether or not to output the ROMized object file.
True: Output the ROMized object file.
False: Do not output the ROMized object file.
|
[Reference]
If the ROMized object file is output: True
If the ROMized object file is not output: False
If the compiler is not supported: None
[Detailed description]
- | This property sets or refers to the setting for output of a ROMized object file, that is, the value of the ROMization process option for the active project. |
[Example of use]
>>>setting = build.ROMization.OutputObjectFile
>>>print setting
True
>>>build.ROMization.OutputObjectFile = False
>>>print build.ROMization.OutputObjectFile
False
|