Operational amplifier
Below is a list of API functions output by the Code Generator for Operational Amplifier use.
Table 3.46 API Functions: [Operational amplifier]
| API Function Name | Function | 
| Performs initialization necessary to control the operational amplifier. | |
| Performs user-defined initialization relatede to the operational amplifier. | |
| Enables operational amplifier reference current circuit. | |
| Disables operational amplifier reference current circuit. | |
| Starts operational amplifier of unit n. | |
| Stops operational amplifier of unit n. | |
| Starts precharging of the external capacitor of the operational amplifier n. | |
| Performs user-defined initialization relatede to the operational amplifier n. |