Temperature sensor
Below is a list of API functions output by the Code Generator for temperature sensor use.
Table 3.24 API Functions: [Temperature Sensor]
|
API Function Name |
Function |
|
Performs initialization necessary to control the temperature sensor. | |
|
Performs user-defined initialization relating to the temperature sensor. | |
|
Starts measurement of the temperature that uses the temperature sen sor. | |
|
Ends measurement of the temperature that uses the temperature sensor. | |
|
Reset the temperature sensor. | |
|
Halts the clock supplied to the temperature sensor. |