Oscillation stop detector
Below is a list of API functions output by the Code Generator for oscillation stop detector use.
Table 3.44 API Functions: [Oscillation Stop Detector]
| 
       API Function Name  | 
    
       Function  | 
| 
       Performs initialization necessary to control the oscillation stop detector.  | |
| 
       Performs user-defined initialization relating to the oscillation stop detector.  | |
| 
       Performs processing in response to the oscillation stop detection interrupt INTOSDC.  | |
| 
       Enables operation of oscillation stop detector.  | |
| 
       Disables operation of oscillation stop detector.  | |
| 
       Halts the clock supplied to the oscillation stop detector.  | |
| 
       Reset the oscillation stop detector.  |