Independent watchdog timer (IWDT)
Below is a list of API functions output by the Code Generator for independent watchdog timer use.
Table 3.24 API Functions: [Independent Watchdog Timer]
| 
       API Function Name  | 
    
       Function  | 
| 
       Performs initialization necessary to control the independent watchdog timer.  | |
| 
       Performs user-defined initialization relating to the independent watchdog timer.  | |
| 
       Performs processing in response to the non-maskable interrupt (WUNI).  | |
| 
       Performs processing in response to the non-maskable/maskable interrupt.  | |
| 
       Clears the independent watchdog timer counter and resumes counting.  |