Multi-function timer pulse unit 3 (MTU3)
Below is a list of API functions output by the Code Generator for multi-function timer pulse unit 3 use.
Table 3.13 API Functions: [Multi-Function Timer Pulse Unit 3]
|
API Function Name |
Function |
|
Performs initialization necessary to control the multi-function timer pulse unit 3. | |
|
Performs user-defined initialization relating to the multi-function timer pulse unit 3. | |
|
Performs processing in response to the input capture/compare match interrupt. | |
|
Performs processing in response to the input capture/compare match interrupt. | |
|
Performs processing in response to the overflow interrupt. | |
|
Performs processing in response to the overflow interrupt. | |
|
Performs processing in response to the underflow interrupt. | |
|
Starts counting by a 16-bit timer. | |
|
Ends counting by a 16-bit timer. |