This function saves the coverage data. [Simulator]
[Specification format]
debugger.Upload.Coverage(fileName, force = False)
|
[Argument(s)]
|
|
|
|
fileName
|
Specify a file name.
|
|
force
|
Specify whether to overwrite.
True: Overwrite
False: Do not overwrite (default).
|
[Return value]
If the memory data was uploaded successfully: True
If there was an error when uploading the memory data: False
[Detailed description]
- | This function saves the coverage data to a file. |
[Example of use]
>>>debugger.Upload.Coverage("C:/test/coverageData.csrcv")
True
>>>
|