|
debugger.Memory.WriteRange
|
This function writes multiple data to the memory.
[Specification format]
debugger.Memory.WriteRange(address, valuelist, memoryOption = MemoryOption.Byte)
|
[Argument(s)]
|
|
|
|
address
|
Specify the start address to write.
|
|
valuelist
|
Specify the list of the value to set.
|
|
memoryOption
|
Specify the unit to set.
The units that can be specified are shown below.
|
|
|
|
|
MemoryOption.Byte
|
Byte unit (8 bits) (default)
|
|
MemoryOption.HalfWord
|
Half-word unit (16 bits) [RH850,RX,V850]
|
|
MemoryOption.Word
|
Word unit (RL78,78K: 16 bits, RH850,RX,V850: 32 bits)
|
[Return value]
If the memory was written to successfully: True
If there was an error when writing to the memory: False
[Detailed description]
- | This function writes, in accord with the setting of memoryOption, the list of values specified by valuelist to the address range starting at the address specified by address. |
[Example of use]
>>> mem = [0x10, 0x20, 0x30]
>>>debugger.Memory.WriteRange(0x100, mem, MemoryOption.Byte)
True
>>>debugger.Memory.ReadRange(0x100, 3, MemoryOption.Byte)
0x10 0x20 0x30
>>>debugger.Memory.WriteRange(0x100, mem, MemoryOption.Word)
True
>>>debugger.Memory.ReadRange(0x100, 3, MemoryOption.Word)
0x00000010 0x00000020 0x00000030
|